orange square Setting device

C 6000
Lever Type Hand Tool
The C 6000 is a lever type hand tool that is operator pressure controlled and designed to install RIVNUT® fasteners. It features
a plunger rotation knob for spin on and spin off of the RIVNUT®.

Installation Sequence
Retract the plunger knob fully and hold the threads of the
RIVNUT® against the mandrel.
While holding the RIVNUT® steady push the plunger in
threading the RIVNUT® fully onto the mandrel with the head
against the anvil.
Place the RIVNUT® into the hole and squeeze the handles of
the tool together until the RIVNUT® forms its backside flange.
Pull the plunger from the tool unthreading from the installed
RIVNUT®.
kameraRiveting in the spindle stroke principle

C 7000
Single Lever Type Hand Tool
The C 7000 is a lever type hand tool that is operator pressure controlled and designed to install RIVNUT® PN fasteners. It features a plunger rotation knob for spin on and spin off of the RIVNUT® PN.

Installation Sequence
Retract the plunger knob fully and hold the threads of the
RIVNUT® PN against the tool mandrel.
While holding the RIVNUT® PN steady push the plunger in
threading the RIVNUT® PN fully onto the tool mandrel with the
head against the anvil nosepiece.
Place the RIVNUT® PN into the hole and squeeze the
handles of the tool together until the RIVNUT® PN forms is
backside legs against the parent material.
Pull the plunger from the tool unthreading from the installed
RIVNUT® PN.
kameraRiveting in the spindle stroke principle
BRK 10
Double Lever Type Hand Tool
The BRK 10 is a double lever type hand tool that is stroke distance controlled by means of an adjustable stop. Once the stroke distance is set the tool will install the RIVNUT® or RIVSTUD® in a single thickness material. The tool also features a plunger rotation knob for spin on and spin off of the product.

Installation Sequence
Retract the plunger knob fully and hold the threads of the
RIVNUT® against the tool mandrel.
While holding the RIVNUT® steady push the plunger in
threading the RIVNUT® onto the tool mandrel with the
RIVNUT® head against the tool anvil nose piece.
Place the RIVNUT® into the hole and squeeze the handles of
the tool together until the mechanical stroke stop of the tool is
reached.
Pull the plunger from the tool unthreading from the installed
product.
kameraRiveting in the spindle stroke principle


letzte Änderung dieser Seite am 29.01.2006