|
Technology | |||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||
| Installation To start with, a frame can be inserted in the opening of the panelling part, if the latter does not permit gliding, if a tolerance compensation is required or for design reasons. The frame is inserted in the opening (1) with its front first. Then press down the frame and allow it to engage (2). Subsequently guide the handling surface into the frame (3) with the latch up front. Exert slight pressure on the symbol surface to engage the shell handle into its final position (4), both lateral support ridges assuming the guiding function. Simple manual actuation permits the opening and closing of the corresponding cladding part, assisted by the spring action. | |||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||
Material
| |||||||||||||||||||||||||||||||||||||||||
Dimensional example
| |||||||||||||||||||||||||||||||||||||||||
Slide fastener