| SONICSERT® is a cylindrical threaded insert with knurled surface and groove, subsequently to be heat- or inductively embedded in thermoplastic synthetic materials. The external diameter is oversized in relation to the insertion bore. Applying radiant heat or an electromagnetic field, the metallic body is brought to melting temperature of the synthetic material. The heat transfer plasticizes the synthetic material within a small threshold-range, filling the cavities and undercuts. A low-strain tight fit is the result after cooling. | ||||||||||||||
| ||||||||||||||