orange square Ultrasonic (USS)

USS (ultrasonic welding) was originally developed for joining thermoplastic mouldings. The plastic material is plasticized very rapidly through friction between the mating surface and vibration absorption of the parts to be combined. This is then followed by the actual joining process. The required energy is produced by the ultrasonic generator in the form of an AC voltage which is converted into mechanical vibration (20 – 40 kHz) and then applied to the parts by a vibrator (sonotrode). The molten material is displaced into recesses and undercuts as the threaded inserts (metal parts size M2 – M6) are installed in the thermoplastic.

Suitable Böllhoff threaded inserts: HITSERT® 2, HITSERT® 3 and SONICSERT®
Insertion tools
Equipment typesRange of sizesEconomic batch size
Hand-operated ultrasonic welding gunM2 - M6<= 5.000
Semi-automatic ultrasonic welding machineM2 - M8<= 50.000
Ultrasonic welding componentsM2 - M8> 10.000
Semi-automatic ultrasonic welding machine
Hand-operated ultrasonic
welding gun
Ultrasonic generator
Ultrasonic transducer
Dimensions:
Possible:
Recommended:
M2 - M6 for metal inserts
M2 - M12 specially plastic in plastic-inserts
Insertion time:
Approx. 2 seconds
Special features:
High noise levels when fitting metal inserts
Considerable abrasion when fitting metal inserts
Unsuitable for threaded bolts
Can easily be converted to other insert sizes
Materials:
Thermoplastics


letzte Änderung dieser Seite am 29.01.2006