orange square SPREDSERT® with retaining flange

Technology

  • For thermoset and thermoplastic components
  • Heavy-duty thread in through holes
  • Screw gripping
    Material: Cu Zn 38 Pb 2
Principle
The SPREDSERT® with retaining flange is placed in the through hole from the underside until the flange is seated. At this point, the slotted, diamond-knurled anchoring section is compressed. When a screw is inserted, the diamond-knurled section of the threaded insert is forced open and the diamond knurling bites into the plastic. The retaining flange acts as a shoulder and provides a high degree of protection against pull-out. Screw locking is also achieved via this process.
The tightening torque is to be increased by 10% for the additional expansion force.
Types
Type 0835

Locating hole



letzte Änderung dieser Seite am 29.01.2006