orange square Pull-out values and test methods

Determining the mechanical values is done in close agreement with the respective client on the basis of a Böllhoff company standard.


Pull out force
[N]

Torque
[Nm]

Jack out
[Nm]
Original components, or trial plates furnished with original Böllhoff materials in the context of advance quality planning, may be used in these required setting trials.
Apart from SONICSERT® thread inserts, other anchoring concepts in the realm of AMTEC® miniature inserts have proven their value.
HITSERT® 3Conical insert (universal) for heat or inductive embedding, tapping, cold insert, optimized feed, self-centering, dismountable
SLIDE PIN Ø 1,0
(stainless steel)
HITSERT® 3
M1,6 x 2,5
Rivet coupling
RIVNUT®
Rivet and flared tube end couplings for thin-walled sheet metal components (e.g. shield plate, SIM card fixture or PCB’s, PWB’s)
M1,6 x 2,8
(brass)
M0,6 x 1,4
(nickel silver)
SNAPLOC® miniSmall synthetic fasteners, made of fibre glass reinforced plastic, subsequent joining with friction welding, heat rivets, purpose-made design, snap-fit connection
SNAPLOC®
pin (PCGF) friction welding
SNAPLOC® coupling(PAGF) heat rivet


letzte Änderung dieser Seite am 29.01.2006